MOTOR.RTYPE

General Information

Type

NV Parameter

Description

Defines the type of thermal resistor inside the motor.

Units

N/A

Range

0 to 1

For firmware version 01-10-02-000 and later, range is 0 to 255.

Default Value

0

Data Type

Integer

Start Version

M_01-00-00-000

Description

This parameter defines the type of thermal resistor used inside of the motor to measures motor temperature.

For firmware versions prior to 01-10-02-000, parameter range is 0 to 1.

0 = PTC

1 = NTC

For firmware versions 01-10-02-000 and later, parameter range is 0 to 255.

0 = Single PTC Thermistor

1 = Single NTC Thermistor

2 = KTY83-110 Thermistor

3 = KTY84-130 Thermistor

4 = PTC + KTY83-110 Thermistors

5 = Thermal switch

255 = No thermal sensorA sensor is a type of transducer that converts one type of energy into another for various purposes including measurement or information transfer in the motor

Related Topics

Motor

 


Stay Connected with Kollmorgen

Copyright © 2015 Kollmorgen™