|
General Information |
|
|---|---|
|
Type |
NV Parameter |
|
Description |
|
|
Units |
V |
|
Range |
50 to 1,000 V |
|
Default Value |
230 V |
|
Data Type |
U16 |
|
See Also |
|
|
Start Version |
M_01-03-00-000 |
Description
This parameter configures the drive for the induction motor's rated voltage as indicated on the nameplate.
MOTOR.VOLTRATED is used to calculate the constant Volts per Hertz characteristics of the drive and motor.
If MOTOR.AUTOSET = 1 and FB1.MEMVER > 0.01, this parameter will be automatically configured for Kollmorgen motors.
Related Topics
|
Copyright © 2015 Kollmorgen™ |
|