REGEN.REXT

General Information

Type

NV Parameter

Description

Sets the external, user-defined regen resistor resistance.

Units

Range

0 to 255

Default Value

0

Data Type

Integer

See Also

N/A

Start Version

M_01-00-00-000

Description

REGEN.REXT sets the external user-defined regen resistor resistance. This variable is needed for the regen resistor temperature estimation algorithm.

Related Topics

Regeneration

 


Stay Connected with Kollmorgen

Copyright © 2015 Kollmorgen™