|
General Information |
|
|---|---|
|
Type |
NV Parameter |
|
Description |
|
|
Units |
Hz |
|
Range |
0 to 10,000 Hz |
|
Default Value |
5,000 Hz |
|
Data Type |
Float |
|
Start Version |
M_01-00-00-000 |
|
Index/Subindex |
Object Start Version |
|
|---|---|---|
|
5000h/0 |
M_01-00-00-000 |
Description
AIN.CUTOFF sets the break frequency in Hz for two cascaded single-pole low-pass filters on the hardware command input. Since the two poles are cascaded at the same frequency, the -3 dB frequency is 0.64*AIN.CUTOFF in hertz and the 10% to 90% step response rise time is 0.53/AIN.CUTOFF in seconds.
Suggested operating values are as follows:
Related Topics
|
Copyright © 2015 Kollmorgen™ |
|