|
General Information |
|
|---|---|
|
Type |
R/O Parameter |
|
Description |
|
|
Units |
V |
|
Range |
-12.5 to +12.5 V |
|
Default Value |
N/A |
|
Data Type |
Float |
|
Start Version |
M_01-00-00-000 |
Variants Supported
|
Index/Subindex |
Object Start Version |
|
|---|---|---|
|
3470h/4 3509h/0 |
M_01-00-00-000 |
Description
AIN.VALUE reads the analog input value after the value is filtered (as shown in the Analog Input Block Diagram).
Related Topics
Block Diagram for Position/Velocity Loop
|
Copyright © 2015 Kollmorgen™ |
|