AOUT.ISCALE

General Information

Type

NV Parameter

Description

Sets the analog current scale factor.

Units

A/V

Range

0.001 to 22.4 A/V

Default Value

0.001 to 22.4 A/V

Data Type

Float

Start Version

M_01-01-01-000

FieldbusA Fieldbus is an industrial network system for real-time distributed control (e.g. CAN or Profibus). It is a way of connecting instruments in a plant design

Index/Subindex

Object Start Version

EtherCATEtherCAT is an open, high-performance Ethernet-based fieldbus system. The development goal of EtherCAT was to apply Ethernet to automation applications which require short data update times (also called cycle times) with low communication jitter (for synchronization purposes) and low hardware costs COE and CANopen

5009h/0

M_01-00-00-000

Description

AOUT.ISCALE sets the analog current scale factor that scales the analog output (AOUT.VALUE) for AOUT.MODE = 4 or 5. The value entered is the motor current per 10 V of analog input or output. This value may be either higher or lower than 100%, but the actual analog I/O will be limited by the application current limit (IL.LIMITN and IL.LIMITP ).

Related Topics

Analog Output

AOUT.ISCALE (➜ p. 1)

 


Stay Connected with Kollmorgen

Copyright © 2015 Kollmorgen™