|
General Information |
|
|---|---|
|
Type |
NV Parameter |
|
Description |
Sets the width-type for a Compare setpointSetpoint is the target value that an automatic control system, for example PID controller, will aim to reach. |
|
Units |
None |
|
Range |
Argument 1: 0 to 7 Argument 2: 0 (position) to 1 (time) |
|
Default Value |
0 |
|
Data Type |
Argument 1:Integer Argument 2: Integer |
|
Start Version |
M_01-13-00-000 |
Compare functionality is supported on hardware revisions D, DB, DA, and higher depending on the drive type. Check the label on the side of the drive to ensure the AKD meets one of the following requirements.
| AKD Type | Hardware Revision Supported |
|---|---|
| AKD | Revision D or higher |
| PDMM | Revision DB or higher |
| AKD-T-IC"Integrated Circuits" Miniaturized electronic circuits (consisting mainly of semiconductor devices, as well as passive components) that have been manufactured in the surface of a thin substrate of semiconductor material | Revision DA or higher |
| FieldbusA Fieldbus is an industrial network system for real-time distributed control (e.g. CAN or Profibus). It is a way of connecting instruments in a plant design | Index/Subindex | Object Start Version | |
|---|---|---|---|
| 34ACh/1 | CMP0.WIDTHTYPE 0 | M_01-13-00-000 | |
| 34AAh/2 | CMP0.WIDTHTYPE 1 | ||
| 34AAh/3 | CMP0.WIDTHTYPE 2 | ||
| 34AAh/4 | CMP0.WIDTHTYPE 3 | ||
| 34AAh/5 | CMP0.WIDTHTYPE 4 | ||
| 34AAh/6 | CMP0.WIDTHTYPE 5 | ||
| 34AAh/7 | CMP0.WIDTHTYPE 6 | ||
| 34AAh/8 | CMP0.WIDTHTYPE 7 | ||
|
34BCh/1 |
CMP1.WIDTHTYPE 0 | ||
|
34BAh/2 |
CMP1.WIDTHTYPE 1 | ||
|
34BAh/3 |
CMP1.WIDTHTYPE 2 | ||
|
34BAh/4 |
CMP1.WIDTHTYPE 3 | ||
|
34BAh/5 |
CMP1.WIDTHTYPE 4 | ||
|
34BAh/6 |
CMP1.WIDTHTYPE 5 | ||
|
34BAh/7 |
CMP1.WIDTHTYPE 6 | ||
|
34BAh/8 |
CMP1.WIDTHTYPE 7 | ||
Description
Use this keyword to set the width-type for a Compare setpoint. The width-type determines whether the width of the Compare pulse is in position counts or units of time (microseconds).
Example
The following example sets the width type of setpoint 7 to microseconds, and the width of setpoint 7 to 1000 microseconds.
-->CMP0.WIDTHTYPE 7 1
-->CMP0.WIDTH 7 1000
Related Topics
|
Copyright © 2015 Kollmorgen™ |
|