This content is not applicable to KAS, using either a PAC"Programmable Automation Controller" PAC is a compact controller that combines the features and capabilities of a PC-based control system with that of a typical programmable logic controller (PLC). A PAC thus provides not only the reliability of a PLC, but also the task flexibility and computing power of a PC. Additionally, because they function and communicate over popular network interface protocols, PACs are able to transfer data from the machines they control to other machines and components in a networked control system or a PDMM.
| FieldbusA Fieldbus is an industrial network system for real-time distributed control (e.g. CAN or Profibus). It is a way of connecting instruments in a plant design | Index/Subindex | Object Start Version |
|---|---|---|
|
5416h/0 |
M_01-14-06-001 |
Description
This parameter stores the position of the upper end of the range where cogging compensation is active on a linear axis.
When the value is changed while compensation values are configured, the compensation values will be redistributed over the new range, which will most likely lead to incorrect compensation.
Before starting COGCOMP.TEACH on a linear axis, the value in COGCOMP.RANGEHIGH has to be larger than COGCOMP.RANGELOW.
Related Topics
|
Copyright © 2015 Kollmorgen™ |
|