COGCOMP.SAVE

This content is not applicable to KAS, using either a PAC"Programmable Automation Controller" PAC is a compact controller that combines the features and capabilities of a PC-based control system with that of a typical programmable logic controller (PLC). A PAC thus provides not only the reliability of a PLC, but also the task flexibility and computing power of a PC. Additionally, because they function and communicate over popular network interface protocols, PACs are able to transfer data from the machines they control to other machines and components in a networked control system or a PDMM.

General Information

Type

Command

Description

Writes the cogging compensation table to non-volatile memory.

Units

N/A

Range

N/A

Default Value

N/A

Data Type

N/A

Start Version

M_01-14-07-000

Description

This parameter saves the current cogging compensation table (COGCOMP.CORRECTIONTABLE) from RAM to NV memory. On next drive boot, the cogging compensation table will be initialized with the stored entries from NV.

Related Topics

 

 


Stay Connected with Kollmorgen

Copyright © 2015 Kollmorgen™