CS.TO

General Information

Type

NV Parameter

Description

Sets the time value for the drive velocity to be within CS.VTHRESH .

Units

ms

Range

1 to 30,000 ms

Default Value

6 ms

Data Type

Integer

Start Version

M_01-00-00-000

FieldbusA Fieldbus is an industrial network system for real-time distributed control (e.g. CAN or Profibus). It is a way of connecting instruments in a plant design

Index/Subindex

Object Start Version

EtherCATEtherCAT is an open, high-performance Ethernet-based fieldbus system. The development goal of EtherCAT was to apply Ethernet to automation applications which require short data update times (also called cycle times) with low communication jitter (for synchronization purposes) and low hardware costs COE and CANopen

3440h/3

M_01-00-00-000

Description

CS.TO is the time value for the drive velocity to be within CS.VTHRESH before the drive disables.

Example

Set time value to 100 ms:

-->CS.TO 100

Related Topics

Controlled Stop

Digital Inputs and Outputs

Fault and Warning Messages

CS.DEC , CS.VTHRESH , CS.STATE, DRV.DIS, DIN1.MODE TO DIN7.MODE, DRV.DISMODE, DRV.DISSOURCES

 

 


Stay Connected with Kollmorgen

Copyright © 2015 Kollmorgen™