DRV.ACTIVE

General Information

Type

R/O Parameter

Description

Reads the enable status of an axis.

Units

N/A

Range

0, 1, 3

Default Value

N/A

Data Type

Integer

Start Version

M_01-00-00-000

Description

DRV.ACTIVE reads the enable status of an axis as follows:

There is no state 2.

When the drive is in state 3, the drive display shows a blinking decimal point.

If an axis is not enabled (DRV.ACTIVE is 0), but DRV.EN is 1 and the hardware enable is high, read the value of DRV.DISSOURCES to query the reason that the drive is not enabled.

Related Topics

Enable/Disable

DRV.EN ,DRV.DISSOURCES

 


Stay Connected with Kollmorgen

Copyright © 2015 Kollmorgen™