|
General Information |
|
|---|---|
|
Type |
R/W |
|
Description |
EnableEnable signal for the drive, Hardware-Enable with 24V signal to X8, Software-Enable command by setup Software, fieldbus or permanently set. Both are required for enabling the drive./disable comparison of motor velocity and maximum emulated encoder velocity. See Fault F486 for details. |
|
Units |
None |
|
Range |
0, 1 |
|
Default Value |
0 (disabled) |
|
Data Type |
Boolean |
|
Start Version |
M_01-06-00-000 |
|
Index/Subindex |
Object Start Version |
|
|---|---|---|
|
520Eh/0 |
M_01-06-00-000 |
Description
Enables comparison of the current motor velocity (or EEO pulse rate for DRV.EMUEMODE 15 to 17) against the maximum speed the emulated encoder output can generate. If the commanded speed exceeds DRV.EMUECHECKSPEED, fault F486 is raised.
| Value | Description |
|---|---|
| 0 | Disabled |
| 1 | Enabled |
Related Topics
DRV.EMUEMODE
|
Copyright © 2015 Kollmorgen™ |
|