DRV.ENDEFAULT

General Information

Type

R/W Parameter

Description

Sets the default state of the software enable.

Units

N/A

Range

0 to 1

Default Value

0

Data Type

Boolean

Start Version

M_01-00-00-000

FieldbusA Fieldbus is an industrial network system for real-time distributed control (e.g. CAN or Profibus). It is a way of connecting instruments in a plant design

Index/Subindex

Object Start Version

EtherCATEtherCAT is an open, high-performance Ethernet-based fieldbus system. The development goal of EtherCAT was to apply Ethernet to automation applications which require short data update times (also called cycle times) with low communication jitter (for synchronization purposes) and low hardware costs COE and CANopen

5080h/0

M_01-00-00-000

Description

DRV. ENDEFAULT sets the default state of the software enable on power up for drives without fieldbusesA Fieldbus is an industrial network system for real-time distributed control (e.g. CAN or Profibus). It is a way of connecting instruments in a plant design (DRV.CMDSOURCE other than 1).

Related Topics

Enable/Disable

 


Stay Connected with Kollmorgen

Copyright © 2015 Kollmorgen™