DRV.FAULTS

General Information

Type

R/O Parameter

Description

Reads the active faults.

Units

N/A

Range

N/A

Default Value

N/A

Data Type

N/A

Start Version

M_01-00-00-000

Description

DRV.FAULTS returns a list of all currently active faults in the system, preceded by their fault number which matches the number displayed on the drive display.

To clear the faults, either issue a DRV.CLRFAULTS or issue a DRV.DIS followed by DRV.EN.

If no active faults are in the system, then after executing DRV.CLRFAULTS the value read by DRV.FAULTS is "No faults active".

Example

-->DRV.FAULTS

502: Bus under voltage.

-->

Related Topics

DRV.CLRFAULTS , DRV.FAULTHIST, DRV.CLRFAULTHIST

 


Stay Connected with Kollmorgen

Copyright © 2015 Kollmorgen™