|
General Information |
|
|---|---|
|
Type |
NV Parameter |
|
Description |
Sets the current that will be used during the DRV.ZERO procedure. |
|
Units |
Arms |
|
Range |
DriveControl device for regulating the speed, torque and position of a motor peak currentThe effective value of the peak current to 0 Arms |
|
Default Value |
0 Arms |
|
Data Type |
Float |
|
Start Version |
M_01-00-00-000 |
|
Index/Subindex |
Object Start Version |
|
|---|---|---|
|
5085h/0 |
M_01-00-00-000 |
Description
This parameter sets the current that is used during the DRV.ZERO procedure.
Related Topics
|
Copyright © 2015 Kollmorgen™ |
|