|
General Information |
|
|---|---|
|
Type |
NV Parameter |
|
Description |
|
|
Units |
N/A |
|
Range |
N/A |
|
Default Value |
No-Name |
|
Data Type |
String |
|
Start Version |
M_01-00-00-000 |
|
Index/Subindex |
Object Start Version |
|
|---|---|---|
|
2031h/0 |
M_01-00-00-000 |
Description
You can assign a unique name to any drive under the following conditions:
- Only use ASCII characters
- Max length of 10 characters
- No spaces in name
This name is one way to identify the drive in a multiple drive network (for instance, in a TCP/IP network on which multiple drives reside).
From the terminal screen, DRV.NAME returns the name of the drive as ASCII characters.
|
Copyright © 2015 Kollmorgen™ |
|