|
General Information |
|
|---|---|
|
Type |
Command |
|
Description |
|
|
Units |
N/A |
|
Range |
N/A |
|
Default Value |
N/A |
|
Data Type |
N/A |
|
Start Version |
M_01-00-00-000 |
|
Index/Subindex |
Object Start Version |
|
|---|---|---|
|
35FEh/0 |
M_01-00-00-000 |
*For Profinet, write a value of 0 into the PNU to execute a command.
Description
This command stops drive motion. In torqueTorque is the tendency of a force to rotate an object about an axis. Just as a force is a push or a pull, a torque can be thought of as a twist and velocity modes, the command value will immediately be set to 0. In position mode, the axis will decelerate to a full stop. If the position command is from a gearing master, the drive will cancel gearing and decelerate to a stop. This command has no effect if the command source is an analog input.
If the command values are coming from a fieldbus master, the stop may be immediately overwritten by a new fieldbus command. Use a controlled stop input or disable command to ensure a stop.
The following table defines the behavior of DRV.STOP:
| Cmdsource | Opmode | Subopmode | Deceleration ramp defined by: |
|---|---|---|---|
| Service | TorqueTorque is the tendency of a force to rotate an object about an axis. Just as a force is a push or a pull, a torque can be thought of as a twist | - | IL"Instruction list" This is a low-level language and resembles assembly.CMD = 0 |
| Velocity | - | If SM.DEC is equal to 0, DRV.DEC is used. Otherwise, SM.DEC is used. | |
| Position | Service motion | If SM.DEC is equal to 0, DRV.DEC is used. Otherwise, SM.DEC is used. | |
| Motion tasking | MT.DEC | ||
| HomingThe Homing procedure allows, based on a position measurement, to set a position offset to the motor in order to ensure it is physically at the home position | HOME.DEC | ||
| Fieldbus | Torque | - | Command has no effect. |
| Velocity | |||
| Position | |||
| Electronic Gearing | Position | - | GEAR.DECMAX |
| Analog | Torque | - | Command has no effect. |
| Velocity | |||
| Position |
|
Copyright © 2015 Kollmorgen™ |
|