|
General Information |
|
|---|---|
|
Type |
R/O Parameter |
|
Description |
|
|
Units |
°C |
|
Range |
55 to 125 °C |
|
Default Value |
N/A |
|
Data Type |
String |
|
Start Version |
M_01-00-00-000 |
|
Index/Subindex |
Object Start Version |
|
|---|---|---|
|
3610h/0 3611h/0 |
M_01-00-00-000 |
Description
DRV.TEMPERATURES reads the temperature in different parts of the drive (power and control boards). The temperature is read from temperature sensors located in the drive.
Example
Below is an example of the output for this command :
Control Temperature: 39 °C
Power1 Temperature: 31 °C
Power2 Temperature: SensorA sensor is a type of transducer that converts one type of energy into another for various purposes including measurement or information transfer does not exist.
Power3 Temperature: Sensor does not exist.
|
Copyright © 2015 Kollmorgen™ |
|