FAULTx.ACTION

General Information

Type

R/W

Description

Gets/Sets the Fault Action for Fault 130, 131, 132, 134, 139, 451, and 702.

Units

N/A

Range

0 to 1

Default Value

0

Data Type

Integer

Start Version

M_01-04-16-000

FieldbusA Fieldbus is an industrial network system for real-time distributed control (e.g. CAN or Profibus). It is a way of connecting instruments in a plant design Index/Subindex Object Start Version

EtherCATEtherCAT is an open, high-performance Ethernet-based fieldbus system. The development goal of EtherCAT was to apply Ethernet to automation applications which require short data update times (also called cycle times) with low communication jitter (for synchronization purposes) and low hardware costs COE and CANopen

5259h/0 FAULT130.ACTION M_01-04-16-000
525Ah/0 FAULT131.ACTION
525Bh/0 FAULT132.ACTION
525Ch/0 FAULT134.ACTION

5267h/0

FAULT451.ACTION
525Dh/0 FAULT702.ACTION

Description

This Parameter determines the action the drive should take when Fault 130, 131, 132, 134, 139, 451, or 702 occurs.

Parameter Value DriveControl device for regulating the speed, torque and position of a motor Action
0 DisableRemoval of the ENABLE signal. Disables power stage. Ampllifier
1 Ignore (fault will not be reported)

 


Stay Connected with Kollmorgen

Copyright © 2015 Kollmorgen™