|
General Information |
|
|---|---|
|
Type |
NV Parameter |
|
Description |
Sets number of successful synchronized cycles needed to lock the PLL. |
|
Units |
N/A |
|
Range |
0 to 10,000 |
|
Default Value |
0 |
|
Data Type |
Integer, U32 |
|
See Also |
Appendix B: FieldbusA Fieldbus is an industrial network system for real-time distributed control (e.g. CAN or Profibus). It is a way of connecting instruments in a plant design Manuals |
|
Start Version |
M_01-00-00-000 |
|
Fieldbus |
Index/Subindex |
Object Start Version |
|---|---|---|
|
50B1h/0 |
M_01-00-00-000 |
Description
This parameter sets number of successful synchronized cycles needed to lock the PLL.
|
Copyright © 2015 Kollmorgen™ |
|