IL.CMD

General Information

Type

R/O Parameter

Description

Reads the value of the q-component current command.

Units

Arms

Range

± DriveControl device for regulating the speed, torque and position of a motor peak currentThe effective value of the peak current (DRV.IPEAK)

Default Value

N/A

Data Type

Float

See Also

DRV.IPEAK

Start Version

M_01-00-00-000

Description

IL"Instruction list" This is a low-level language and resembles assembly.CMD displays the q-component current command value of the current loop after any limitation (such as a parameter setting or I2t calculation).

IL.CMD is limited also by motor peak current, IL.LIMITN and IL.LIMITP .

Related Topics

Current Loop

 


Stay Connected with Kollmorgen

Copyright © 2015 Kollmorgen™