|
General Information |
|
|---|---|
|
Type |
R/O Parameter |
|
Description |
|
|
Units |
Arms |
|
Range |
0 to 500 Arms |
|
Default Value |
DriveControl device for regulating the speed, torque and position of a motor peak currentThe effective value of the peak current (DRV.IPEAK) |
|
Data Type |
Float |
|
See Also |
Foldback |
|
Start Version |
M_01-00-00-000 |
|
Index/Subindex |
Object Start Version |
|
|---|---|---|
|
3420h/0 |
M_01-00-00-000 |
Description
IL"Instruction list" This is a low-level language and resembles assembly.FOLDFTHRESH is the fault level of the current foldback algorithm. If IL.IFOLD drops below the value for IL.FOLDFTHRESH, then a fault is generated and the drive is disabled.
To avoid reaching the current foldback fault level, set IL.FOLDFTHRESHU well below the continuous current value for both the drive and the motor or set the IL.FOLDFTHRESHU value to zero.
Related Topics
|
Copyright © 2015 Kollmorgen™ |
|