|
General Information |
|
|---|---|
|
Type |
NV parameter |
|
Description |
|
|
Units |
N/A |
|
Range |
0 to 1 |
|
Default Value |
0 |
|
Data Type |
Integer |
|
See Also |
|
|
Start Version |
M_01-04-01-000 |
|
Index/Subindex |
Object Start Version |
|
|---|---|---|
|
3427h/1 |
M_01-00-00-000 |
Description
This parameter determines the method of the motor protection.
0 – The motor foldback mechanism is responsible for protecting the motor from overload.
1 – The Motor I2t algorithm is responsible for protecting the motor from overload.
Related Topics
|
Copyright © 2015 Kollmorgen™ |
|