|
General Information |
|
|---|---|
|
Type |
Command |
|
Description |
|
|
Units |
N/A |
|
Range |
N/A |
|
Default Value |
N/A |
|
Data Type |
N/A |
|
See Also |
Communicating with the DriveControl device for regulating the speed, torque and position of a motor |
|
Start Version |
M_01-04-05-000 |
*For Profinet, write a value of 0 into the PNU to execute a command.
Description
When this command is issued a new IP will be acquired using IP.MODE to select what method is used.
Notes:
Recovering communications with a drive on an un-reachable IP address
Sometimes a drive may be configured for an IP Address, and the drive needs to be taken off-line, and bench tested, or otherwise used outside of its saved IP Settings. If IP.MODE has been set to 1 (using software defined static IP), the drive will boot up on an IP Address that may be unreachable with the host computer’s settings.
If the IP address prevents communication the IP settings can be reset to default by the following procedure:
- Set both rotary switches to 0
- Hold down button B1 (top-side of drive) for 5 seconds.
The display will flash 0.0.0.0 and then attempt to discover an address by DHCP. Without removing logic power from the drive, use Workbench to connect to the drive, reconfigure the IP address settings as desired, and store the values to non-volatile memory.
Related Topics
IP.ADDRESS | IP.GATEWAY | IP.SUBNET | IP.MODE
|
Copyright © 2015 Kollmorgen™ |
|