|
General Information |
|
|---|---|
|
Type |
NV Parameter |
|
Description |
|
|
Units |
N/A |
|
Range |
0 to 510 |
|
Default Value |
6 |
|
Data Type |
Integer |
|
See Also |
|
|
Start Version |
M_01-00-00-000 |
|
Index/Subindex |
Object Start Version |
|
|---|---|---|
|
359Dh/0 |
M_01-00-00-000 |
Description
MOTOR.POLES sets the number of motor poles. This command is used for commutation control and represents the number of individual magnetic poles of the motor (not pole pairs). A motor's magnetic poles range from 0 to 510, which corresponds to 0 to 255 magnetic pole pairs. The division value of motor poles (MOTOR.POLES) and feedback poles (FB1.POLES) must be an integer when setting drive to enable, otherwise a fault is issued.
This parameter is automatically configured for Kollmorgen motors when MOTOR.AUTOSET=1.
Related Topics
|
Copyright © 2015 Kollmorgen™ |
|