PL.CMD

General Information

Type

R/O Parameter

Description

Reads the position command directly from the entry to the position loop.

Units

Depends on UNIT.PLINEAR (pg 1) or UNIT.PROTARY (pg 1)

Rotary: counts, rad, deg, (custom units), 16-bit counts

Linear: counts, mm, µm, (custom units), 16-bit counts

Range

N/A

Default Value

N/A

Data Type

Float

See Also

PL.FB

Start Version

M_01-00-00-000

Description

PL.CMD reads the position command as it is received in the position loop entry.

Related Topics

PL.ERR | PL.ERRFTHRESH | PL.ERRMODE | PL.ERRWTHRESH

Position Loop

 


Stay Connected with Kollmorgen

Copyright © 2015 Kollmorgen™