|
General Information |
|
|---|---|
|
Type |
R/O parameter |
|
Description |
|
|
Units |
Watt |
|
Range |
N/A |
|
Default Value |
N/A |
|
Data Type |
Integer |
|
See Also |
N/A |
|
Start Version |
M_01-00-00-000 |
|
Index/Subindex |
Object Start Version |
|
|---|---|---|
|
3416h/0 |
M_01-00-00-000 |
Description
This parameter reads regen resistor's calculated power, which is determined as follows:
(V2 / R) * DutyCycle
Related Topics
|
Copyright © 2015 Kollmorgen™ |
|