|
Index/Subindex |
Object Start Version |
|
|---|---|---|
|
541fh/0 |
M_01-16-02-000 |
Description
Disables the automatic Wake and Shake procedure if the identified feedback type is sine encoder without halls (FB1.IDENTIFIED = 21) and the encoder pitch is equal to the motor pole pitch of the linear motor.
| Value | Description |
|---|---|
| 0 | enabled |
| 1 | disabled |
Related Topics
|
Copyright © 2015 Kollmorgen™ |
|