|
General Information |
|
|---|---|
|
Type |
R/W Parameter |
|
Description |
|
|
Units |
ms |
|
Range |
1 to 200 ms |
|
Default Value |
2 ms |
|
Data Type |
U8 |
|
See Also |
WS.IMAX , WS.DISTMAX |
|
Start Version |
M_01-01-00-101, M_01-02-00-000 |
|
Index/Subindex |
Object Start Version |
|
|---|---|---|
|
36D0h/0 |
M_01-00-00-000 |
Description
This parameter defines the duration for each different current-vector while the coarse angle calculation. The move distance is proportional to the WS.T and WS.IMAX value.
Related Topics
|
Copyright © 2015 Kollmorgen™ |
|