ID: DINT ID of the string as declared in the string table
Q : STRING Loaded string or empty string in case of error
This function loads a string from the active string table and stores it into a STRING variable. The StringTable() function is used for selecting the active string table.
The "ID" input (the string item identifier) is an identifier such as declared within the string table resource. You don't need to "define" again this identifier. The system does it for you.
Q := LoadString (ID);
See also
|
Copyright © 2015 Kollmorgen™ |
|