SerializeOutPLCopen motion icon

Description

This function copies the value of a variable to a binary frame. This function is commonly used for building a communication frame in binary format.

In LD"Ladder diagram" Ladder logic is a method of drawing electrical logic schematics. It is now a very popular graphical language for programming Programmable Logic Controllers (PLCs). It was originally invented to describe logic made from relays. The name is based on the observation that programs in this language resemble ladders, with two vertical "rails" and a series of horizontal "rungs" between them language, the operation is executed only if the input rung (EN) is TRUE. The output rung (ENO) keeps the same value as the input rung.

The FRAME input must be an array large enough to receive the data. If the data cannot be safely copied to the destination buffer, the function returns 0.

The function copies the following number of bytes to the destination frame:

1 byte BOOL, SINT, USINT and BYTE variables
2 bytes INT, UINT and WORD variables
4 bytes DINT, UDINT, DWORD and REAL variables
8 bytes LINT and LREAL variables

The function returns the position in the destination frame, after the copied data. Thus the return value can be used as a position for the next serialization

Arguments

Input

En Description Execute the function
  Data type BOOL
  Range [0,1]
  Unit n/a
  Default
FrameIn networking dialect, a message is called a frame[] Description Destination buffer - must be an array.
  Data type USINT
  Range [0,+65535]
  Unit n/a
  Default
Data Description Source variable to be copied
  Data type any except STRING
  Range
  Unit n/a
  Default
Pos Description Position in the destination buffer
  Data type DINT
  Range [0,+65535]
  Unit n/a
  Default
BigEndian Description TRUE if the frame is encoded with Big Endian format.
  Data type BOOL
  Range [0,1]
  Unit n/a
  Default

Output

OK Description Returns true when the function successfully executes. See Function - General rules.
  Data type BOOL
  Unit n/a
NextPos Description Position in the destination buffer after the copied data. 0 in case or error (invalid position / buffer size).
  Data type DINT
  Unit n/a

Examples

Structured Text

NextPos := SerializeOut(Frame[](*USINT*), Data(*ANY*), Pos(*DINT*), BigEndian(*BOOL*)); //Read the position

 


Stay Connected with Kollmorgen

Copyright © 2015 Kollmorgen™