REPEAT
<statements>
UNTIL <BOOL expression> END_REPEAT;
The statements between "REPEAT" and "UNTIL" are executed until the Boolean expression is TRUE. The condition is evaluated after the statements are executed. Statements are executed at least once.
Loop instructions can lead to infinite loops that block the target cycle. Never test the state of an input in the condition as the input will not be refreshed before the next cycle.
iPos := 0;
REPEAT
MyArray[iPos] := 0;
iNbCleared := iNbCleared + 1;
iPos := iPos + 1;
UNTIL iPos = iMax END_REPEAT;
Not available
Not available
Not available
See also
|
Copyright © 2015 Kollmorgen™ |
|