TP / TPRPLCopen motion icon

Function BlockA function block groups an algorithm and a set of private data. It has inputs and outputs. - PulseWhen the step gets activated, the action is activated for a single execution, and possibly once again when the step is deactivated timer.

Inputs

IN : BOOL   Timer command
PT : TIME   Programmed time

RST : BOOL  ResetNew start of the microprocessor (TPR only)

Outputs

Q : BOOL   Timer elapsed output signal
ET : TIME  Elapsed time

Time diagram

TpDiag.gif (2861 octets)

Remarks

The timer starts on a rising pulse of IN input. It stops when the elapsed time is equal to the programmed time. A falling pulse of IN input resets the timer to 0, only if the programmed time is elapsed. All pulses of IN while the timer is running are ignored. The output signal is set to TRUE while the timer is running.

TPR is same as TP but has an extra input for resetting the timer

In FFLD language, the input rung is the IN command. The output rung is Q the output signal.

ST Language

(* MyTimer is a declared instance of TP function block *)
MyTimer (IN, PT);
Q := MyTimer.Q;
ET := MyTimer.ET;

FBD Language

TpFbd.gif (1221 octets)

FFLD Language

TpLd.gif (1345 octets)

IL Language:

(* MyTimer is a declared instance of TP function block *)
Op1: CAL MyTimer (IN, PT)
     FFLD  MyTimer.Q
     ST  Q
     FFLD  MyTimer.ET
     ST  ET

See also

TON   TOF   BLINK

 


Stay Connected with Kollmorgen

Copyright © 2015 Kollmorgen™