Limits

This screen allows you view and modify the various drive limits.

Button or Dialog Box

Description

Parameter

Current Limits

 

 

Positive Peak Current

The maximum positive current allowed.

IL.LIMITP

Negative Peak Current

The maximum negative current allowed.

IL.LIMITN

Dynamic Break Peak Current The maximum amplitude of the current for dynamic braking. DRV.DBILIMIT

Velocity Limits

 

 

Positive Speed Limit

The maximum speed allowed in the positive direction.

VL.LIMITP

Negative Speed Limit

The maximum speed allowed in the negative direction.

VL.LIMITN  

User Over Speed Limit

The user set threshold velocity for an over speed fault.

VL.THRESH

Overall Over Speed Limit The overall over speed fault threshold. VL.VFTHRESH

Acceleration Limits

 

 

Acceleration

The acceleration ramp used to profile some types of motion.

DRV.ACC

Deceleration

The deceleration ramp used to profile some types of motion.

DRV.DEC

Motor Limits

Motor limits are set through the Motor Foldback Screen (see Foldback)

 

Limits

The limits screen covers most of the basic system limits, including current, velocity, and position.

 


Stay Connected with Kollmorgen

Copyright © 2015 Kollmorgen™