Motion Library - Cam Profile
-
-
For a description of the this pipe block and its parameters, see Pipe Blocks Description
| Name | Description | Return type |
| MLCamInit |
Initializes a cam Pipe Block with user-defined settings |
BOOL |
| MLCamSwitch |
Switches profiles of the selected cam object |
BOOL |
| MLPrfReadIOffset |
Returns the Input Offset value of a selected cam profile |
None |
| MLPrfReadIScale |
Returns the Input Ratio value of a selected cam profile |
None |
| MLPrfReadOOffset |
Returns the Output Offset value of a selected cam profile |
None |
| MLPrfReadOScale |
Returns the Output Ratio value of a selected cam profile |
None |
| MLPrfWriteIOffset |
Sets the Input Offset value of a selected cam profile |
BOOL |
| MLPrfWriteIScale |
Sets the Input Ratio value of a selected cam profile |
BOOL |
| MLPrfWriteOOffset |
Sets the Output Offset value of a selected cam profile |
BOOL |
| MLPrfWriteOScale |
Sets the Output Ratio value of a selected cam profile |
BOOL |
| MLProfileBuild | Builds a cam profile from application data | See Output |
| MLProfileCreate |
Creates a new cam profile object |
None |
| MLProfileInit |
Initializes a previously created cam profile object |
BOOL |
| MLProfileRelease | Removes a Profile so the Profile ID may be used by a different or new Profile. | See Output |