Function Block MCFB_JogPLCopen motion icon

Description

This function block is defined to jog an axis in the selected direction at a defined speed. The En input (FFLD editor only) must be high. Typically wired to the rail.

The AxisID selects the axis to jog. The JogPlus and JogMinus inputs select the direction the motion will occur in. Only one of these inputs should be enabled at a given time. If both are selected the motion will stop. If other motion is active when the jog is requested that motion will be aborted and the jog will start.

The following figure shows the function block I/O

UDFB Jog for PLCopen

Figure 7-215: Jog for PLCopen

 

Arguments

Input

En

Description

Enables execution (FFLD only )

 

Data type

BOOL

 

Range

—

 

Unit

n/a

 

Default

—

AxisID

Description

ID Name of the Axis

 

Data type

DINT

 

Range

—

 

Unit

n/a

 

Default

—

JogPlus

Description

Enables a Jog in the plus direction

 

Data type

BOOL

 

Range

[0 , 1]

 

Unit

n/a

 

Default

—

JogMinus

Description

Enables a Jog in the Minus direction

 

Data type

BOOL

 

Range

[0 , 1]

 

Unit

n/a

 

Default

—

Speed

Description

Rate at which the axis will move

 

Data type

LREAL

 

Range

—

 

Unit

User unit/sec

 

Default

—

Accel Decel

Description

Linear Acc/Dec rate

 

Data type

LREAL

 

Range

—

 

Unit

User unit/sec2

 

Default

—

Output

InMotion

Description

Jogging is active when TRUE

 

Data type

BOOL

 

Unit

n/a

Usage

This function Block is used to command motion in a designated direction at a defined rate. This may be used where continuous motion required as in a conveyor system, or in a setup mode for manually jogging the axis. Motion will start when the JogPlus or JogMinus input is true. It will stop when the input goes false.

Related Functions

MC_MoveVelocity

Example

Structured Text

 

InMotion := Inst_Jog_PLCopenClosedA vendor -and product- independent worldwide association active in Industrial Control and aiming at standardizing PLC file formats based on XML(Axis1, Switch_1, Switch_2, 600, 10000);

 

Ladder Diagram

UDFB Jog PLCopen: LD example

Function Block Diagram

UDFB Jog PLCopen: FBD example

Go back to the top of the page [Top]