SD Card Access
Files may be written to and read from an SD card. This is typically used for storing a firmware image for Recovery Mode.
To use an SD card on the controller:
- Ensure that the SD card is inserted
- Mount the card using SD_MOUNT
- Ensure the card is accessible using SD_ISREADY before performing a read or write action
- Unmount the card, if desired, using SD_UNMOUNT after performing read/write actions