UDP Functions for PDMM/PCMM & Simulator
UDP (User Datagram Protocol) is a communications protocol which allows computers to exchange messages across an IP network. The UDP functions listed below provide a KAS controller to communicate with a remote PC or another KAS controller over an Ethernet
Ethernet is a large, diverse family of frame-based computer networking technologies that operate at many speeds for local area networks (LANs) network.
When a UDP packet is sent to a broadcast address such as '255.255.255.255', the AKD PDMM or PCMM automatically converts the given broadcast address to the broadcast address of its Ethernet interface. For example if the controller's IP address is 192.168.1.10 and the subnet mask is 255.255.255.0, then the controller's Ethernet interface broadcast address is 192.168.1.255.
| Function | Description |
|---|---|
| udpAddrMake | Build an address buffer for UDP functions |
| udpClose | Close a socket |
| udpCreate | Create a UDP socket |
| udpIsValid | Test if a socket is valid |
| udpRcvFrom | Receive a telegram |
| udpRcvFromArray | Receive a byte array through UDP |
| udpRcvFromVar | Receives the contents of a variable through UDP |
| udpSendTo | Send a telegram |
| udpSendToArray | Send a byte array through UDP |
| udpSendToVar | Sends the contents of a local variable through UDP |
-
-
See Wikipedia for more information on the UDP protocol.