Show Pipe Network and Profiles-Generated Code
You can access the code equivalent to the graphical representation with the contextual menu of the Pipe Network item in the Project Explorer as follows:
Figure 4-16: Display Source Code of the Pipe Network
The KAS IDE
"Integrated development environment"
An integrated development environment is a type of computer software that assists computer programmers in developing software.
IDEs normally consist of a source code editor, a compiler and/or interpreter, build-automation tools, and a debugger provides a set of Functions and function blocks for each of the Pipe Blocks. These function blocks allow the logic part of the application to control and interact with the motion engine.