PDO Content
This section lists the objects within the currently selected PDO. Objects may be created (Add Object), modified (Edit Object), or removed from the project (Delete Object). Select a PDO in the Editable PDOs section (left side of dialog box) to view the objects in a PDO. The list of objects will appear in the PDO Content section (right side of dialog box).![]()
| Index | Identification value for the PDO. The range is defined by the EtherCAT RxPDOs: 0x1600 to 0x17FF TxPDOs: 0x1A00 to 0x1BFF |
| Name | Text label to identify the PDO. The name is provided either by the device vendor or user, and can be changed by the user. |
| Size [bytes] | Total length for the PDO object(s) data. |
| User Modified | Yes: indicates the user has changed the PDO or its content No: indicates the PDO is the default provided by the device vendor. |
-
-
Constraints for the Kollmorgen AKD device family: The PDO content Size field will be highlighted in red if the Editable PDO content size is greater than 8 bytes.