PDMM/PCMM EDS file for EtherNet/IP
The KAS installation contains an EtherNet/IP EDS file for the Kollmorgen controller. This file may be needed by other controllers, (PLCs, PCs etc.) to configure the EtherNet/IP communication with a AKD PDMM.
The KAS_Controller_EIP.eds file is located in the \Astrolabe\Bin\EDS directory, where the KAS software was installed. By default, the EDS file is located:
C:\Program Files (x86)\Kollmorgen\Kollmorgen Automation Suite\Astrolabe\Bin\EDS\KAS_Controller_EIP.eds
| Revision | Compatibility | Change |
|---|---|---|
| 1.0 | KAS v2.7 only | Initial revision |
| 1.1 | KAS v2.8 only | Updated vendor information |
| 1.2 | KAS v2.9 only | Support up to 4 input and output assemblies when KAS Runtime |
Table 7-3: Revision history for AKD PDMM EDS file for EtherNet/IP