AXIS#.HOME.DIR
Description
AXIS#.HOME.DIR is the initial direction used when homing starts.
| Value | Description |
|---|---|
| 0 | Movement in negative direction. |
| 1 |
Movement in positive direction. |
Versions
| Action | Version | Notes |
|---|---|---|
| Implemented | 02-00-00-000 |
General Information
This content is not applicable to KAS.
|
Type |
Read/Write |
|
Units |
N/A |
|
Range |
0 to 1 |
|
Default Value |
1 |
|
Data Type |
Integer |
|
See Also |
N/A |
|
Stored in Non Volatile Memory |
Yes |
Variants Supported
All variants are supported.
Fieldbus Information
| Fieldbus |
Parameter | Index | Sub-Index | Data Type | Float Scale | Units | Access | PDO Mappable |
|---|---|---|---|---|---|---|---|---|
| EtherCAT |
AXIS1.HOME.DIR | 0x5008 | 0x3 | UINT | - | - | RW | False |
| AXIS2.HOME.DIR | 0x5108 | 0x3 | UINT | - | - | RW | False |
Related Topics
Homing