AXIS#.HWEN.STATE
Description
This parameter returns the state of the hardware enable input.
If AXIS#.HWEN.SOURCE=0, indicating that no hardware enable input is configured, AXIS.HWEN.STATE always returns 1.
Usage
0: Hardware enable input is low preventing the axis from being enabled.
1: Hardware enable input is high allowing the axis to be enabled.
Versions
| Action | Version | Notes |
|---|---|---|
| Implemented | 02-00-00-000# |
General Information
| Type | Read Only |
| Units | N/A |
| Range | 0 to 1 |
| Default Value | N/A |
| Data Type | Integer |
| See Also | AXIS#.HWEN.SOURCE, AXIS#.HWEN.MODE |
|
Stored in Non Volatile Memory |
No |
Variants Supported
All variants are supported.
Fieldbus Information
| Fieldbus |
Parameter | Index | Sub-Index | Data Type | Float Scale | Units | Access | PDO Mappable |
|---|---|---|---|---|---|---|---|---|
| EtherCAT |
AXIS1.HWEN.STATE | 0x5009 | 0x3 | USINT | - | - | RO | False |
| AXIS2.HWEN.STATE | 0x5109 | 0x3 | USINT | - | - | RO | False |