AXIS#.HWLS.NEGSOURCE

Description

Selects which digital input will be used as the negative limit switch input for an axis.

No negative limit switch input is configured if this is set to zero.

Examples

Usage

0 (default): no negative limit switch input configured

1 to 8: selects DIN# as the negative limit switch input for an axis and is supported on all drive models.

9 to 12: selects DIN# as the negative limit switch input for an axis on drives with X22 Extended I/O Connector

Code

Selects DIN7 as the negative limit switch input for axis 1 and DIN4 as the input for axis 2.

-->AXIS1.HWLS.NEGSOURCE 7

-->AXIS2.HWLS.NEGSOURCE 4
		

No negative limit switch input is configured for axis 1 and DIN1 is selected as the input for axis 2.

-->AXIS1.HWLS.NEGSSOURCE 0

-->AXIS2.HWLS.NEGSOURCE 1

Context

For more information on limit switches, refer to Limits.

Versions

Action Version Notes
Implemented 02-00-00-000

General Information

Type Read/Write
Units N/A
Range 0 to 8, extended to 12 for drives with X22 Extended I/O Connector
Default Value 0
Data Type Integer
See Also AXIS#.HWLS.NEGSTATE
Stored in Non Volatile Memory Yes

Variants Supported

All variants are supported

Fieldbus Information

FieldbusClosedA Fieldbus is an industrial network system for real-time distributed control (e.g. CAN or Profibus). It is a way of connecting instruments in a plant design Parameter Index Sub-Index Data Type Float Scale Units Access PDO Mappable
EtherCATClosedEtherCAT is an open, high-performance Ethernet-based fieldbus system. The development goal of EtherCAT was to apply Ethernet to automation applications which require short data update times (also called cycle times) with low communication jitter (for synchronization purposes) and low hardware costs COE and CANopen AXIS1.HWLS.NEGSOURCE 0x5015 0x3 USINT - - RW False
AXIS2.HWLS.NEGSOURCE 0x5115 0x3 USINT - - RW False