AXIS#.IL.FOLDFTHRESH
Description
AXIS#.IL
"Instruction list"
This is a low-level language and resembles assembly.FOLDFTHRESH is the fault level of the current foldback algorithm. If AXIS#.IL.IFOLD drops below the value for AXIS#.IL.FOLDFTHRESH, then a fault is generated and the drive is disabled.
To avoid reaching the current foldback fault level, set AXIS#.IL.FOLDFTHRESHU well below the continuous current value for both the drive and the motor or set the AXIS#.IL.FOLDFTHRESHU value to zero.
Versions
| Action | Version | Notes |
|---|---|---|
| Implemented | 02-00-00-000 |
General Information
|
Type |
Read Only |
|
Units |
Arms |
|
Range |
0 to 500 Arms |
|
Default Value |
Drive peak current (IPEAK) |
|
Data Type |
Float |
|
Stored in Non Volatile Memory |
No |
Variants Supported
All variants are supported.
Fieldbus Information
| Fieldbus |
Parameter | Index | Sub-Index | Data Type | Float Scale | Units | Access | PDO Mappable |
|---|---|---|---|---|---|---|---|---|
| EtherCAT |
AXIS1.IL.FOLDFTHRESH | 0x500A | 0x8 | DINT | 1000:1 | - | RO | False |
| AXIS2.IL.FOLDFTHRESH | 0x510A | 0x8 | DINT | 1000:1 | - | RO | False |