AXIS#.IL.LIMITN
Description
This parameter sets the negative user limit clamp value of the torqueTorque is the tendency of a force to rotate an object about an axis. Just as a force is a push or a pull, a torque can be thought of as a twist-producing q-component current command (AXIS#.IL.CMD ). The current command is additionally limited by the motor peak current setting (AXIS#.MOTOR.IPEAK
) and by the present value of the foldback I²t peak motor current protection.
Versions
Action | Version | Notes |
---|---|---|
Implemented | 02-00-00-000 |
General Information
Type |
Read/Write |
Units |
A |
Range |
Negative drive peak current (IPEAK) to 0 A |
Default Value |
Negative drive peak current (IPEAK) |
Data Type |
Float |
See Also |
|
Stored in Non Volatile Memory |
Yes |
Variants Supported
All variants are supported.
Fieldbus Information
Fieldbus![]() |
Parameter | Index | Sub-Index | Data Type | Float Scale | Units | Access | PDO Mappable |
---|---|---|---|---|---|---|---|---|
EtherCAT![]() |
AXIS1.IL.LIMITN | 0x500A | 0x5 | DINT | 1000:1 | - | RW | False |
AXIS2.IL.LIMITN | 0x510A | 0x5 | DINT | 1000:1 | - | RW | False |