AXIS#.MOTOR.BRAKEPOWERLOW
Description
Low voltage used by power saving brake operation (AXISx.MOTOR.BRAKEPOWERSAVING).
-
-
This parameter is automatically configured for Kollmorgen motors when MOTOR.AUTOSET=1 and motor memory version is 0.4 or greater.
Context
For more information see Brake and Motor.
Versions
Action | Version | Notes |
---|---|---|
Implemented | 02-00-00-000 |
General Information
Type |
Read/Write |
Units |
Volts |
Range |
10.602 to 24.002 |
Default Value |
17 |
Data Type |
Float |
Stored in Non Volatile Memory |
Yes |
Variants Supported
All variants are supported.