AXIS#.MT.V
Description
AXIS#.MT.V specifies the motion task velocity, which is used by the and command. This parameter is a temporary value. A motion task is only set after an command. The motion task velocity is furthermore limited by AXIS#.VL.LIMITP or AXIS#.VL.LIMITN depending on the direction of the motion task.
A value of 0 should not be used when setting a motion task via because this value causes a validity check of the command to fail.
A value of 0 after an command displays an empty (not initialized) motion task.
Examples
Code
Sets the velocity of motion task 0 to 60 RPM
"Revolutions per minute"
Is a unit of frequency of rotation: the number of full rotations completed in one minute around a fixed axis. It is used as a measure of rotational speed of a mechanical component. The first parameter is the motion task number and the second is the velocity.
-->AXIS1.MT.V 0 60
Versions
| Action | Version | Notes |
|---|---|---|
| Implemented | 02-00-00-000 |
General Information
This content is not applicable to KAS.
|
Type |
Read/Write |
|
Units |
Rotary: RPM, RPS, deg/s, (custom units)/s, rad/s See Velocity Units for details. |
|
Range |
Depends on units. See Velocity Range for details. |
|
Default Value |
0 RPM Depends on units. See Velocity Units for details. |
|
Data Type |
Float |
|
Stored in Non Volatile Memory |
Yes |
Variants Supported
All variants are supported.
Related Topics
Motion Tasks