AXIS#.PL.FILTERTIME

Description

AXIS#.PL.FILTERTIME sets the period of a second order lowpass on the trajectory position command. When AXIS#.PL.FILTERTIME is greater than zero, the filter is active. The filter is applied to all Command Source types, but only active when the drive is in Position Mode.

This feature is typically used for smoothing abrupt changes in position command, or filtering coarse command steps from low resolution controllers, or electronic gearing.

Versions

Action Version Notes
Implemented 02-00-00-000

General Information

Type

Read/Write

Units

Milliseconds

Range

No range limitation

Default Value

0

Data Type

Float

Stored in Non Volatile Memory

Yes

Variants Supported

All variants are supported.