AXIS#.UNIT.ACCROTARY
Description
AXIS#.UNIT.ACCROTARY sets the acceleration/deceleration units when the motor type (AXIS#.MOTOR.TYPE ) is rotary.
| Type | Description |
|---|---|
|
0 |
|
|
1 |
RPS/s |
|
2 |
deg/s2 |
|
3 |
Custom Units/s2 |
| 4 | rad/s2 |
Versions
| Action | Version | Notes |
|---|---|---|
| Implemented | 02-00-00-000 |
General Information
|
Type |
Read/Write |
|
Units |
N/A |
|
Range |
0 to 4 |
|
Default Value |
0 |
|
Data Type |
Integer |
|
See Also |
|
|
Stored in Non Volatile Memory |
Yes |
Variants Supported
All variants are supported.
Fieldbus Information
| Fieldbus |
Parameter | Index | Sub-Index | Data Type | Float Scale | Units | Access | PDO Mappable |
|---|---|---|---|---|---|---|---|---|
| EtherCAT |
AXIS1.UNIT.ACCROTARY | 0x5010 | 0x3 | USINT | - | - | RW | False |
| AXIS2.UNIT.ACCROTARY | 0x5110 | 0x3 | USINT | - | - | RW | False |